Technical FAQs

Ask a Question

What is the part number for replacement handle only for a VC2GU?

KCF1PZ can be used to replacement the original handle assembly. However, please note the original factory supplied shaft must be used with the replacement handle. The standard replacement handle shaft will be too short to properly engage the switch and if used, could cause the switch to disengage from the handle assembly during normal use.


CTA-ID : 13156
Was this helpful?
What can we do to improve the information ?