Technical FAQs

Ask a Question

If a QO240GFI is used on a load without a neutral, will the test circuit still function?

Yes it would as long as the breaker pigtail was connected to the panel neutral

CTA-ID : 13155
Was this helpful?
What can we do to improve the information ?