Technical FAQs

Ask a Question

Are the HOMELINE load centers suitable for use on a 48 V DC application?

Issue:
Product Design

Product Line:
Homeline Load Centers

Environment:
Voltage System

Cause:
Application

Resolution:

No, the HOMELINE load centers are not suitable for use on any DC system. Consider using the QO load centers


CTA-ID : 12836
Was this helpful?
What can we do to improve the information ?