Technical FAQs

Ask a Question

QOB-SWN Circuit Breakers is the Neutral line also opened?

Yes. Phase and neutral conductors are opened when the Breaker is in the off or tripped position


CTA-ID : 12833
Was this helpful?
What can we do to improve the information ?