Technical FAQs

Ask a Question

What are the repair parts for the H362RBWC, series F1? (may be shown as F01)

Only the parts listed below are considered field repairable.
Line Base Assy - 4056603850 (Does not include Arc Suppressor).
Arc Supressor Assy - 4056635550
Load Base Assy - 4056604050
Lug kit - AL0306F (includes 6 lugs, mounting hardware and instructions)
Handle/Mechansm Kit - HMR0306FN1 (Replace both the handle and mechanism if either one needs repair).

CTA-ID : 13147
Was this helpful?
What can we do to improve the information ?