Technical FAQs

Ask a Question

Are the handles used with the GS1 and LK3 disconnect switches suitable for outdoor use?

Beginning September 1, 2002, these handles are approved and UL Listed NEMA 4/4X indoor/outdoor.


CTA-ID : 13138
Was this helpful?
What can we do to improve the information ?