Technical FAQs

Ask a Question

Is an ATS46C66N considered to be NEMA 1enclosed ?<br /><br /><br />

No. These units have live terminals which are not finger safe and are exposed to contact.

All are NEMA Open:
The ATS 46D17N to 46C14N starters are considered IP20 rated.
The ATS 46C17N to 46M12N starters are considered IP00 rated.

The ATS23 U70N to C15N starters are considered IP20 rated.
The ATS23 C24N to M12N starters are considered IP00 rated.

The unit should be put in an appropriately sized enclosure if desire to obtain a NEMA 1 rating.


CTA-ID : 12831
Was this helpful?
What can we do to improve the information ?