Technical FAQs

Ask a Question

Does the ATV28 include a keypad?

Issue:  Does the ATV28 include a keypad?
 
Product Line:  ATV28
 
Environment:  All
 
Cause:  N/A
 
Resolution:  Yes. The non-removable keypad for the Altivar 28 drive is for display and adjustment. It does not have start and stop functions.

The available remote keypad (part number VW3A28101) does have start/stop cabability.


 
Was this helpful?
What can we do to improve the information ?