Technical FAQs

Ask a Question

What Main Breaker is used in a EZM31600CB?

A PAF2036 circuit breaker frame with PA31600RC rating columns is used as the Main Breaker in this device.


CTA-ID : 13337
Was this helpful?
What can we do to improve the information ?