Technical FAQs

Ask a Question

What Main Breaker is used in a EZM31200CB?

A PAF2036 circuit breaker frame with PA31200RC rating columns is used as the Main Breaker in this device..


CTA-ID : 13335
Was this helpful?
What can we do to improve the information ?