Technical FAQs

Ask a Question

What Main Breaker is used in a EZM11200CB?

A PAF2026 circuit breaker frame with PA21200RC rating columns is used as the Main Breaker in this device.


CTA-ID : 13334
Was this helpful?
What can we do to improve the information ?