Technical FAQs

Ask a Question

What are the repair parts for the H222N, series F1? (may be shown as F01).

The repair parts for the H222N, series F1 (F01) are as follows. No other parts are available.

Interior Kit - HSIF2206F (includes line & load base assemblies, arc suppressor, mechanism, mounting hardware and instructions)
Load Base kit - HLB2603206F (includes load base, mounting hardware and instructions)
Arc Suppressor kit - HAS0610F (includes arc suppressor, mounting hardware and instructions)
Lug kit - AL0306F (includes 6 lugs, mounting hardware and instructions)
Handle/Mechanism kit - HM0610F (includes handle, handle gasket, mechanism, lockplate, mounting hardware and instructions)
Handle Assembly - use handle/mechanism kit
Lockplate - use handle/mechanism kit
Neutral Assembly - SN0610
Neutral Bonding Screw - 40283-456-51 (Obsolete - replaced by 40283-656-50)



CTA-ID : 13010
Was this helpful?
What can we do to improve the information ?