Technical FAQs

Ask a Question

Can the operating handle of a MA1000DS circuit breaker enclosure be padlocked in the OFF position?

Yes, the external operating handle is provided with an integral lockplate for padlocking the handle in the OFF position.
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 OR P1200 SERIES OF ENCLOSURES.


CTA-ID : 12810
Was this helpful?
What can we do to improve the information ?