Technical FAQs

Ask a Question

What Main Breaker is used in a EZM3800CBU?

Issue:
What is the main breaker that is installed in the EZM3800CBU?

Product Line:
Commercial metering products sold and supported in the USA.

Environment;
Product features

Cause:
Breaker determination

Resolution:
If the EZM3800CBU is older, the main breaker was the old MHF36800.  If the EZM3800CBU is of current design, the main breaker is the Powerpact MGF36800. 



 
Was this helpful?
What can we do to improve the information ?