Technical FAQs

Ask a Question

What are the repair parts for the H663AWK, series F3? (may be shown as F03)

Issue:
Repair parts

Product Line:
Heavy Duty Safety Switch

Cause:
Maintenance

Resolution:
The repair parts for the H663AWK, series F3 (F03) are as follows. No other parts are available.

Interior Kit - HSIF6610CF (includes line and load base Assemblies, mechanism, arc suppressor, all mtg. hardware and instructions).
Load Base Kit - HLB310CF- TWO kits required (includes load base, mounting hardware and instructions).
Arc Suppressor Kit - HAS0610F- TWO kits required (includes arc suppressor, mtg. hardware and instructions).
Lug Kit - CL10F -TWO kits required (includes 6-lugs and mtg. hardware).
Handle/Mechanism Kit - HM0610F (includes handle, mechanism, lockplate, gasket, all mtg. hardware and instructions).


CTA-ID : 13114
Was this helpful?
What can we do to improve the information ?