Technical FAQs

Ask a Question

What are the repair parts for the H663AWK, series F1? (may be shown as F01)

The repair parts for the H663AWK, series F1 (F01) are as follows. No other parts are available.

Interior Kit - HSIF6610CF (includes line and load base Assemblies, mechanism, arc suppressor, all mtg. hardware and instructions).
Load Base Kit - HLB310CF- TWO kits required (includes load base, mounting hardware and instructions).
Arc Suppressor Kit - HAS0610F- TWO kits required (includes arc suppressor, mtg. hardware and instructions).
Lug Kit - CL10F -TWO kits required (includes 6-lugs and mtg. hardware).
Handle/Mechanism Kit - HM0610F (includes handle, mechanism, lockplate, gasket, all mtg. hardware and instructions).


CTA-ID : 13113
Was this helpful?
What can we do to improve the information ?