Technical FAQs

Ask a Question

What are the repair parts for the H222N, series F4? (may be shown as F04).

The repair parts for the H222N, series F4 (F04) are as follows. No other parts are available.

Line Base Assembly -40566-421-50 (requires one per switch. Arc suppressor assembly not included)
Load Base Assembly - 40560-026-50 (requires one per switch)
Arc Suppressor Assembly - 40560-018-01 (requires one per switch)
Lug Assembly - 40251-016-52 (per lug)
Switch Mechanism - 40566-107-50
Handle Assembly - 4056684150K
Lockplate - 40566-376-01
Neutral Assembly - SN03
Neutral Bonding Screw - 40283-456-51 (Obsolete - replaced by 40283-656-50)
Line & Load base mounting screws - 40205-160-01 (3 for line & 2 for load)
Arc suppressor mtg screw - 40205-145-01 (1 required)
Lockplate mtg. screw - 22999-405-62 (2 required)


CTA-ID : 13006
Was this helpful?
What can we do to improve the information ?