Technical FAQs

Ask a Question

Is there a hand held programmer for Model 98 temperature controller?

There is not a hand held programmer for this device; however, it is possible to program from the front of the device, or using a laptop with software and a RS485 connection.


CTA-ID : 12799
Was this helpful?
What can we do to improve the information ?