Technical FAQs

Ask a Question

What is the wire range of the lugs used in an EZM3400TB tap box?<br />

Standard Lugs for an EZM3400TB will accommodate:
(2) 3/0 AWG - 500 kcmil AL/CU wires per Phase and Neutral, and
(1) #6 AWG - 300 kcmil AL/CU Ground wire.



CTA-ID : 13294
Was this helpful?
What can we do to improve the information ?