Technical FAQs

Ask a Question

What is the wire range of the lugs used in a EZM11600TB?

The line phase and neutral lugs accept (6) #2 AWG - 600 kcmil Al/Cu conductors per phase.


CTA-ID : 13293
Was this helpful?
What can we do to improve the information ?