Technical FAQs

Ask a Question

What are the repair parts for the H361-2A, series F1? (may be shown as F01)

The repair parts for the H361-2A, series F1 (F01) are as follows. No other parts are available.

Complete Interior kit - HSIF3603206CF (Includes line & load base assemblies, arc suppressor, mechanism, all mounting hardware and instructions)
Load Base kit - HLB3603206CF (includes load base, mtg. hardware & instructions)
Arc Suppressor kit - HAS0610F (includes arc suppressor, mtg. hardware & instructions)
Lug kit - CL0306F (includes 6 lugs, mtg. hardware & instructions)
Handle/Mechanism kit - HM0610F (includes handle, mechanism, gaskets, lockplate, mtg. hardware & instructions)



CTA-ID : 12998
Was this helpful?
What can we do to improve the information ?