Technical FAQs

Ask a Question

Do Vario switches have screw terminals?

Yes, however, they are loose in the box and must be installed by the customer with the screws facing the direction desired, depending on whether the device is to be panel mounted or door mounted. If the terminals are discarded with the box, the customer must buy a new switch, as the terminals are not available as a spare part.

CTA-ID : 12776
Was this helpful?
What can we do to improve the information ?