Technical FAQs

Ask a Question

What is the wire range of the Main Switch lug used in a EZM3400FS?

An LHP36000M Molded Case Switch is used as the Main Switch in this device. The line lugs accept (1) 1/0 AWG - 600 kcmil or (2) 1/0 AWG - 250 kcmil Al/Cu conductors per phase. The same range is provided on the neutral lug.


CTA-ID : 13281
Was this helpful?
What can we do to improve the information ?