Technical FAQs

Ask a Question

What are the repair parts for the H223AWK, series F3? (may be shown as F03)

The repair parts for the H223AWK, series F3 (F03) are as follows. No other parts are available.

Interior Kit - HSIF210CF (includes line and load base Assemblies, mechanism, arc suppressor, all mtg. hardware and instructions).
Load Base Kit - HLB210CF (includes load base, mounting hardware and instructions).
Arc Suppressor Kit - HAS0610F (includes arc suppressor, mtg. hardware and instructions).
Lug Kit - CL10F (includes 6-lugs and mtg. hardware).
Handle/Mechanism Kit - HM0610F (includes handle, mechanism, lockplate, gasket, all mtg. hardware and instructions).


CTA-ID : 13101
Was this helpful?
What can we do to improve the information ?