Technical FAQs

Ask a Question

What are the repair parts for the H321AWK, series F1? (may be shown as F01)

Issue:
What are the repair parts for the H321AWK, series F1? (may be shown as F01)

Product Line:
Heavy Duty Safety Switch

Environment:
Replacement parts

Cause:
Maintenance required

Resolution:
The repair parts for the H321AWK, series F1 (F01) are as follows. No other parts are available.

Line Base Assembly -40566-428-50 (requires one per switch. Arc suppressor assembly not included)
Load Base Assembly - 40566-412-50 (requires one per switch)
Arc Suppressor Assembly - 40560-018-01 (requires one per switch)
Lug Assembly - CL0306F (includes 6 lugs)
Switch Mechanism - 40566-107-50
Handle Assembly - 4056684150K
Handle Gasket - 40566-031-01
Lockplate - 40566-376-01
Line & Load base mounting screw - 40205-160-01 (3 for line & 2 for load)
Arc Suppressor mounting screw - 40205-145-01 (1 required)
Lockplate mounting screw - 22999-405-62 (2 required)


CTA-ID : 12993
Was this helpful?
What can we do to improve the information ?