Technical FAQs

Ask a Question

What are the replacement parts for the H221A, series F1? (may be shown as F01)

The replacement parts for the H221A, series F1 (F01) are as follows. No other parts are available.

Line Base Assembly -40566-427-50 (requires one per switch. Arc suppressor assembly not included)
Load Base Assembly - 40566-408-50 (requires one per switch)
Arc Suppressor Assembly - 40560-018-01 (requires one per switch)
Lug Assembly - CL0306F (includes 6 lugs)
Switch Mechanism - 40566-107-50
Handle Assembly - 4056684150K
Handle Gasket - 40566-031-01
Lockplate - 40566-376-01
Line & Load base mounting screw - 40205-160-01 (3 for line & 2 for load)
Arc Suppressor mounting screw - 40205-145-01 (1 required)
Lockplate mounting screw - 22999-405-62 (2 required)


CTA-ID : 12989
Was this helpful?
What can we do to improve the information ?