Technical FAQs

Ask a Question

Can the cover of a MA1000AWK circuit breaker enclosure be padlocked closed?

Yes, the cover is provided with an integral padlock hasp for locking the cover closed.
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 OR P1200 SERIES OF ENCLOSURES.


CTA-ID : 12772
Was this helpful?
What can we do to improve the information ?