Technical FAQs

Ask a Question

How many contact blocks can be mounted on the XB2 operators?

Non illuminated devices can be configured with 6 contacts maximum, mounted side by side and stacked 3 deep. Illuminated devices can have 4 contacts, mounted side by side and stacked 2 deep.


CTA-ID : 12760
Was this helpful?
What can we do to improve the information ?