Technical FAQs

Ask a Question

What is the standard wire range of the Main Switch lugs used in the EZM1400FS?

Standard Terminal Lug Data

Product Line:
EZM Metering

EZM Main lugs

Standard terminations


The LHP26000M Molded Case Switch is used as the Main Switch in this device. The line lugs accept (1) 1/0 AWG - 600 kcmil or (2) 1/0 AWG - 250 kcmil Al/Cu conductors per phase. The same range is provided on the neutral lug.

CTA-ID : 13277
Was this helpful?
What can we do to improve the information ?