Technical FAQs

Ask a Question

Can solid state overload modules be used for ground fault protection on a 200hp unit for example?

When we provide ground fault relay (940GAT12 & 940GA375T) on line side of the starter to feed both starter and bypass the solid state overload relay with ground fault will not work since the overload function of the relay is sensitive to the harmonic distortion of starter.


CTA-ID : 13275
Was this helpful?
What can we do to improve the information ?