Technical FAQs

Ask a Question

Why are the fuses recommended for ATS46 enclosed units so much higher than what is recommended for standard units?

The fuses in the enclosure are not sized to protect soft start from high currents but to contain damage within the unit if got a catostrophic failure.
When Ir is set properly the unit protects itself from excessive currents.


CTA-ID : 13272
Was this helpful?
What can we do to improve the information ?