Technical FAQs

Ask a Question

What concerns do you need to take into consideration when oversizing a soft start?

Oversizing is possible but need to be careful not to oversize to a point where unit does not see at least 10% current draw of its nominal rating (this is a must) Certain features also may not work as expected like current limit and may need external overload protection.

CTA-ID : 13270
Was this helpful?
What can we do to improve the information ?