Technical FAQs

Ask a Question

What are the repair parts for the HU463 series F3? (may be shown as F03)

Repair Part

Product Line:
Heavy Duty Safety Switch


The repair parts for the HU463, series F3 (F03) are as follows. No other parts are available.

Interior kit - HSIU4610F (Includes line & load base assemblies, mechanism, arc suppressor, all mounting hardware and instructions).
Arc Suppressor kit - HAS0610F - (TWO required, includes arc suppressor & mounting hardware)
Lug kit - AL10F - (TWO required, kit includes 6 lugs)
Handle/Mechanism kit- HM0610F (kit includes handle, mechanism, lockplate & mounting hardware)

CTA-ID : 13096
Was this helpful?
What can we do to improve the information ?