Technical FAQs

Ask a Question

What are the repair parts for the HU463 series F1? (may be shown as F01)

Issue:
Repair Part

Product Line:
Heavy Duty Safety Switch

Cause:
Maintenance

Resolution:
The repair parts for the HU463, series F1 (F01) are as follows. No other parts are available.

Interior kit - HSIU4610F (Includes line & load base assemblies, mechanism, arc suppressor, all mounting hardware and instructions).
Arc Suppressor kit - HAS0610F - (TWO required, includes arc suppressor & mounting hardware)
Lug kit - AL10F - (TWO required, kit includes 6 lugs)
Handle/Mechanism kit- HM0610F (kit includes handle, mechanism, lockplate & mounting hardware)


CTA-ID : 13095
Was this helpful?
What can we do to improve the information ?