Technical FAQs

Ask a Question

What are the repair parts for the HU363RB series F1? (may be shown as F01)

Issue:
Repair Parts

Product Line:
Heavy Duty Safety Switch

Cause:
Maintenance

Resolution:
The repair parts for the HU363RB, series F1 (F01) are as follows. No other parts are available.

Interior kit - HSIU3610F (Includes line & load base assemblies, mechanism, arc suppressor, all mounting hardware and instructions).
Arc Suppressor kit - HAS0610F - (includes arc suppressor & mounting hardware)
Lug kit - AL10F - (kit includes 6 lugs)
Handle/Mechanism kit- HM0610F (kit includes handle, mechanism, lockplate & mounting hardware)



CTA-ID : 13093
Was this helpful?
What can we do to improve the information ?