Technical FAQs

Ask a Question

What are the repair parts for the H461, series F5? (may be shown as F05)

The repair parts for the H461, series F5 (F05) are as follows. No other parts are available.

Complete interior - HSIF4603F (includes, line & load base assembly, arc suppressor assembly, mechanism, all mounting hardware and instruction sheets)
Load Base assembly - HLB2603203F (2-required inlcudes mtg hardware)
Arc suppressor assembly - HAS0610F (2-required includes mtg hardware)
Lug Assembly - AL0306F (2-required includes mtg hardware)
Mechanism Assembly - HM0610F (includes mechanism, handle, lockplate and handle gaskets)
Handle assembly - use mechanism assembly
Lockplate - use mechanism assembly


CTA-ID : 12984
Was this helpful?
What can we do to improve the information ?