Technical FAQs

Ask a Question

Can Merlin Gerin Multi 9 supplementary protectors breakers be used with the AK5 Bus Bar System - part number; AK5PA232 mounting plate tap-off? <br /><br />Application; Customer is building a control panel. <br /><br />

Merlin Gerin Multi 9 supplementary protectors can be used with the AK5 bus bar system. As long as the din rail used is a 35mm, 7.5 mm depth, they will fit.





CTA-ID : 12979
Was this helpful?
What can we do to improve the information ?