Technical FAQs

Ask a Question

When does the fan on the softstarter to turn on?

On the units smaller than ATS46D75N there are no fans.
On ATS46D75N and larger the fans are operated by a thermal switch that turns them on at 50*C.


CTA-ID : 13267
Was this helpful?
What can we do to improve the information ?