Technical FAQs

Ask a Question

What are the PIV rating for the rectifiers and IGBTs used in the drives?

For the 460v units the rectifiers are rated for 1600v and the IGBTs are 1200v. For the 230v units the rectifiers are rated for 1600v and the IGBTs are 600v.


CTA-ID : 13260
Was this helpful?
What can we do to improve the information ?