Technical FAQs

Ask a Question

What is the accuracy of the keypad display?

The keypad accuracy is around 5% and if desire better accuracy would look at the AO which is 0.6% accurate.


CTA-ID : 13259
Was this helpful?
What can we do to improve the information ?