Technical FAQs

Ask a Question

Why does the unit trip out on memory failure?

This fault can occur if running on a low line condition. Make sure don`t have extremely dirty line power. J5 may be loose also which could cause non communication and initiate fault. If the fault persist, change out the control card.

CTA-ID : 13255
Was this helpful?
What can we do to improve the information ?