Technical FAQs

Ask a Question

How would you wire in a safety shut down so that motor would stop in either drive or bypass mode?

If want to stop the unit in either drive or bypass mode would need to wire in a contact to break the 120v from the transformer so that neither the isolation nor bypass contactors can remain closed and not be able to pull in. The motors will perform a free wheel stop when the contacts open.

CTA-ID : 13253
Was this helpful?
What can we do to improve the information ?