Technical FAQs

Ask a Question

What are the repair parts for a PAK10CTG, Series E02, ServicePak Power Outlet Panel?

Only the parts listed below are considered field replaceable.
Cover - 4054005101
Cover Mounting Screws - 2142717161 (2 req`d)
Interior Trim - 4054021101
Interior Trim Mounting Screw - 4020513001K (2 req`d)
Interior Assembly - 4054018451 (Includes the Base Assy, Circuit Breaker(s) and Receptacle(s) listed below)
Base Assembly - 4054010650
Circuit Breaker - QO120GFI
Receptacle - 4054001450
Receptacle Mounting Screw - 2190312160 (2 req`d)
Receptacle Mounting Spring Clip - 2330100001 (2 req`d per receptacle)
Neutral Bonding Screw - Not Applicable
Ground Bar - 4023089855
Ground Bar Mounting Screw - 2159414200
Closing Cap - BCAP
Closing Cap Mounting Screw - 2142720241 (2 req`d)
Note: Covers and Interior Trims do not have labels applied.


CTA-ID : 12971
Was this helpful?
What can we do to improve the information ?