Technical FAQs

Ask a Question

What is set screw security on a 9001 KR24 and KR25 mushroom push button?

Knob is held in place by an Allen Wrench set screw in addition to the threads of the knob onto the operator.


CTA-ID : 13533
Was this helpful?
What can we do to improve the information ?