Technical FAQs

Ask a Question

What does the S4 in part number 9001 KM38S4 indicate?

This is a 9001 KM38 light module modified with a 5 Kohm resistor installed in so that a 24 volt GE #1843 lamp can be used.

CTA-ID : 13517
Was this helpful?
What can we do to improve the information ?