Technical FAQs

Ask a Question

Why does the auto / manual functionality in menu 7.2 not work when have unit in PI control?

The auto / manual in menu 7.2 is non-compatible with PI control and to operate with auto / manual functionality have to set this up through the PI parameter for auto / manual. When have auto/manual programmed in setpoint manual it allows you to when logic input is high, manual is selected and when logic input is low, auto is selected.

CTA-ID : 13249
Was this helpful?
What can we do to improve the information ?