Technical FAQs

Ask a Question

Can the XMLF be fitted with a tamper proof cover?

The clear plastic front cover and the corresponding upper right corner of the housing are drilled out to accept a fine wire which can be sealed with a crimped seal. No separate cover is available.

CTA-ID : 12962
Was this helpful?
What can we do to improve the information ?