Technical FAQs

Ask a Question

What are the location ratings for a 9036DR31 ?

These products are rated NEMA 7 & 9 which places them for Class I/Division I & II / Groups C & D as well as Class II/ Divs I & II / Groups E,F & G per Product Data A84 p. 2

CTA-ID : 12961
Was this helpful?
What can we do to improve the information ?