Technical FAQs

Ask a Question

What are the repair parts for the H461, series F1? (may be shown as F01)

The repair parts for the H461, series F1 (F01) are as follows. No other parts are available. (NOTE: Descriptions below of ``left side`` and ``right side`` mean your left or right as you face the switch.)

Complete interior - HSIF4603F (includes, line & load base assembly, arc suppressor assembly, mechanism, all mounting hardware and instruction sheets)
Load Base assembly - HLB2603203F (2-required inlcudes mtg hardware)
Arc suppressor assembly - HAS0610F (2-required includes mtg hardware)
Lug Assembly - AL0306F (2-required includes mtg hardware)
Mechanism Assembly - HM0610F (includes mechanism, handle, lockplate and gaskets)

CTA-ID : 12952
Was this helpful?
What can we do to improve the information ?