Technical FAQs

Ask a Question

What legend plate is included in the 9001 AS1?

The 9001 AS1 includes the 9001 KN244 legend, which is marked OFF ON.


CTA-ID : 13494
Was this helpful?
What can we do to improve the information ?